AN4457 UART Emulation - use via CubeMx?
Split from old (2020), abandoned thread: https://community.st.com/t5/stm32cubemx-mcus/uart-emulation-an4457-is-it-possible-to-use-it-via-cubemx/td-p/310812 for better visibility - and to enable marking a solution...
Hi,
I have the same problem, trying to reverse engineer the AN4457 example for an H7xx MCU using with STM32CubeIDE. Currently my problem is that I need to "#define HAL_UART_EMUL_MODULE_ENABLED " in stm32h7xx_hal_conf.h, but there is not "USER CODE" field, so the define gets overwritten each time I change the IOC file.
I guess the proper approach would be to select the UART_EMUL module in the device configuration tool of the GUI, but I do not know how to make it visible there ...
Did anyone implement this example using an IDE? It would be really helpful for the CubeIDE users.
Thanks!