Apparent error on the HAL SPI library when using DMA.
Even after setting up a DMA stream to a SPI_RX DMA request, the HAL_SPI_Receive_DMA() function return error code 1 when called. I've solved this problem by also setting up a DMA stream to the SPI_TX request, even though I won't use it.
Problem occurred when using SPI1 on Full-Duplex Master mode in the STM32F412 uC, STM32CubeIDE Version: 1.16.1