arm_fir_q15() Hard Fault
Hi,
I've a NUCLEO-F767ZI. I'm having problem getting the arm_fir_q15() to work, it gives me a hard fault. I'm defining the variables like this:
#define BLOCK_SIZE 1
#define NUM_TAPS 51
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
uint32_t blockSize = BLOCK_SIZE;
arm_fir_instance_q15 S;
static q15_t firStateQ15[BLOCK_SIZE + NUM_TAPS - 1];
static q15_t firCoeffs[NUM_TAPS] =
{
-93, -88, -77, -60, -34, 0, 44, 97, 161,
235, 319, 412, 513, 620, 732, 847, 961, 1074,
1181, 1281, 1370, 1447, 1509, 1555, 1583, 1592, 1583,
1555, 1509, 1447, 1370, 1281, 1181, 1074, 961, 847,
732, 620, 513, 412, 319, 235, 161, 97, 44,
0, -34, -60, -77, -88, -93
};
uint16_t g_AdcReading[8];
After calling arm_fir_init_q15(&S, NUM_TAPS, (q15_t *)firCoeffs, (q15_t *)firStateQ15, blockSize) and the rest of the HAL stuff in the main() function, it proceeds to the DMA interrupt where the data is processed:
void ADC_DMA_Callback(void)
{
char AsciiData[16] = {0};
float sin = 0;
q15_t sinQ15 = 0;
static float filtSin = 0;
q15_t filtSinQ15 = 0;
for(uint8_t i = 0; i < 8; i++)
sin += g_AdcReading[i];
sin /= 8;
sin *= 8.05861e-4;
arm_float_to_q15(&sin, &sinQ15, blockSize);
arm_fir_q15(&S, &sinQ15, &filtSinQ15, blockSize);
arm_q15_to_float(&filtSinQ15, &filtSin, blockSize);
snprintf(AsciiData, sizeof AsciiData, "%.2f,%.2f\n", sin, filtSin);
HAL_UART_Transmit(&huart3, (uint8_t *)AsciiData, strlen(AsciiData), 1);
}The problem I'm having is that after the call to arm_fir_q15() the system goes to the hard fault loop, giving me this:

If I use arm_fir_f32() with the appropriate float variables, coefficients, etc., it does function normally. What might be causing this hard fault?
Regards,
Helder