AT+CEREG response is "+CEREG: 0,4", where 4 means "Unknown", even when connected to the Network. The modem is LBAD0ZZ1SE in stm32l462re board
I am currently working with TYPE1SE Modem (LBAD0ZZ1SE) in the stm32l462re board. I am having an issue where the modem response to the command AT+CEREG? is "+CEREG: 0,4", where 4 means "Unknown (for example, out of Evolved Terrestrial Radio Access Network (E-UTRAN) coverage)" from what I searched. The modem is connected since I can successfuly PING the NBIOT network. Is there a reason for this response "+CEREG: 0,4" or something I can do to make the response appear as "Registered" instead of "Unkown"?
Thank you in advance for your time and attention.