Azure FileX sd driver issue
Hello ST community,
I believe there is an issue with the code generated by CubeMX for the fx_stm32_sd_driver.
Config used :
- STM32CubeIDE : 1.10.1
- STM32U5 Cube Package : 1.1.1
- STM32CubeMX : 6.6.1
In CubeMX, when I set the "FX Driver Initializes the SD IP" flag to true, the generated code wont compile as the MX_SDMMC1_SD_Init is generated static in the main, so the code below in fx_stm32_sd_driver.c is irrelevant...
#if (FX_STM32_SD_INIT == 1)
extern void MX_SDMMC1_SD_Init(void);
#endif
One solution is to remove the static keyword but every time CubeMX generates code, it comes back and it's kind of unpractical.
Could you please fix that in a future package update ?
Thanks,
Clement