Azure IOT Porting STM32H735G-DK
Hi currently i am using STM32H735G-DK board and i need to integrate with azure IOT via ethernet
1. From .Ioc file i have enabled MQTT,msns,dns,dhcp,sntp,cloud and i have added Nx azure related files and azure c sdk and the file structure as attached in the image
2. If have referred an example in the below link and also links attached
https://github.com/tdjastrzebski/B-L4S5I-IOT01A_AZURE-RTOS
https://github.com/STMicroelectronics/x-cube-azrtos-h7
3. The examples where all are connected with WIFI is there any example with ethernet connectivity or where i can change the things for ethernet connectivity and azure iot
4. i am using
STM32CubeIDE
Version: 1.18.0