AzureRTOS + HTTP WebServer and MULTIPART transfer
Hi All,
I've succesfully implemented an HTTP WebServer into our application running AzureRTOS on a STM32F429.
I'm now moving to data transfer over HTTP, in order to have a Web page (entry point) for transfering a binary file (encrypted) to remote update the board on the field.
The flow is something as follow:
Web Page -> load file (encrypted) -> save file payload in binary on ext flash (in raw, no FS).
Then issue a reboot (bootlaoder will read the file & calculate the crc) and then flash the MCU if everything match.
In order to transfer correctly the file i had to enable NX_HTTP_MULTIPART_ENABLE , but i was wondering if there's a good point to start with some example (docs are not so exaustive).
Right now for receving the file i do :
UCHAR buffer[1440] = { 0 };
if ( strcmp(resource, "/upload.php") == 0 && request_type == NX_WEB_HTTP_SERVER_POST_REQUEST )
{
ULONG len = 0;
ULONG offset = 0;
fwu_start();
while( nx_web_http_server_get_entity_header(server_ptr,&packet_ptr, buffer, sizeof(buffer)) == NX_SUCCESS )
{
while( nx_web_http_server_get_entity_content(server_ptr, &packet_ptr, &offset,&len) == NX_SUCCESS )
{
nx_packet_data_extract_offset(packet_ptr,offset, buffer, len, &len);
buffer[len] = 0;
fwu_raw_write((uint8_t*)buffer, (size_t)len);
}
}
nx_web_http_server_type_get(server_ptr, server_ptr -> nx_web_http_server_request_resource, temp_string, &string_length);
status = nx_web_http_server_callback_generate_response_header(server_ptr, &resp_packet_ptr, NX_WEB_HTTP_STATUS_OK,
0, "", NX_NULL);
if(status == NX_SUCCESS)
{
status =nx_web_http_server_callback_packet_send(server_ptr, resp_packet_ptr);
if(status != NX_SUCCESS)
{
nx_packet_release(resp_packet_ptr);
return status;
}
}
else
{
return NX_SUCCESS;
}
}
Is there any better way to do that? is that the right way?
Thanks all in advance
Davide