Skip to main content
Visitor II
February 24, 2022
Solved

AzureRTOS with CubeMX makefile generates IAR files instead of GNU

  • February 24, 2022
  • 6 replies
  • 2541 views

I'm trying to generate a project using the AzureRTOS software expansion package. When generating code through STM32CubeIDE the correct files are generated (I'm using a GNU ARM compiler), however when I set the Makefile option in CubeMX some files are generated for the IAR system instead of GNU. This causes compilation error. Is there a setting to make sure that the GNU files are generated instead of IAR?

    This topic has been closed for replies.
    Best answer by Sara BEN HADJ YAHYA

    Hello @Hermund Døssland​, @NRedd.2​,

    This issue is fixed in STM32CubeMX latest release.

    V6.7.0 is now available under this Link.

    Thanks for your contribution :smiling_face_with_smiling_eyes:

    Sara.

    6 replies

    ST Employee
    February 25, 2022

    @Sara BEN HADJ YAHYA​, any idea?

    ST Employee
    March 8, 2022

    Hello @Hermund Døssland​ ,

    Sorry for the late reply,

    Could you please share your ioc file?

    thanks,

    Sara.

    HDøss.1Author
    Visitor II
    March 9, 2022

    Hi Sara BEN HADJ YAHYA (Employee),

    Here it is, thanks for looking into it!

    HDøss.1Author
    Visitor II
    March 9, 2022

    @Sara BEN HADJ YAHYA​ 

    ST Employee
    March 9, 2022

    Hello @Hermund Døssland​ ,

    You are right and I confirm the issue, it seems that the IAR folder is generated instead of the GNU folder when a Makefile project is generated.

    I've raised this issue internally to be fixed as soon as possible. I'll keep you posted with the updates.

    Internal ticket number: 124088 (This is an internal tracking number and is not accessible or usable by customers).

    If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

    Thanks for your contribution,

    Sara.

    Graduate II
    June 13, 2022

    Hi,

    This issue still persists in 6.5.0 version.

    Could you please fix it?

    ST Employee
    June 13, 2022

    Hello @NRedd.2​ ,

    The dev team is working on this issue, I will let you know once the fix is done.

    Sara.

    ST Employee
    November 28, 2022

    Hello @Hermund Døssland​, @NRedd.2​,

    This issue is fixed in STM32CubeMX latest release.

    V6.7.0 is now available under this Link.

    Thanks for your contribution :smiling_face_with_smiling_eyes:

    Sara.