B-L475E Azure example
Has anyone gotten the B-L475E-IOT01 board azure sample to build properly. I noticed that it is not set up to do any PostBuild processing. I took the Postbuild step from the F413 board example and put it into the project. It's failing with prepareimage.py (I'm on a mac, but am going to try and do this on a windows machine shortly) sayign that the image is to large to combine with the SBSFU image. I'd be happy with just having a secure firmware image of the Azure application only to upload into it