Blocking a GPIO pin to LOW state
Hi, I have a circuit in which I want to check every cycle if a measured voltage is over a limit value and in that case disable the measure over one of four DUTs forcing to LOW the state of some pins. The problem is that in the main loop I have command line that set the state of the pin sometimes to high and sometimes to low and I would to find a way to block the state of a pin and do not change his state until the end of the program. I thought to use the IF but I have 4 DUTs to check and control separately.