Boot from and execute code from external Single- or Dual-SPI flash memory
Hey. Is it possible to execute code from external memory using only single- or dual-SPI mode? I have a PCB here with a STM32H730 CPU, but on the flash memory, WP/SIO2 and RESET/SIO3 are connected, so no Quad-SPI possible. :frowning_face:
In these official references concerning XiP I only find Quad-SPI or Dual-Quad(=Octo)-SPI mentioned:
- AN5188
- AN4760 section 6.2
- https://www.youtube.com/watch?v=YFIvJVsvIsE&list=PLnMKNibPkDnHIrq5BICcFhLsmJFI_ytvE&index=2
Thank You!