Boot from external flash stm32h755
Hello, I am trying to boot from the external flash memory that the nucleo-h755zi-q has(addres->0x09000000), but I am having some issues. The idea I was following is :
1. Create a Bootloader project, in this project I configure the QuapSPI in the internal flash memory to memory mapped mode
2. create the App project (with a basic toggleLed) changing the .ld flash direction to the 0x09000000. Once the project is created I get back to the Bootloader and in debug configurations I linked the Bootloader with the App, so when the Bootloader is debugged the App will too.
3. In the Bootloader file I created a function called 'JumpToAplication' that tries to Jump to the app when the quadspi is done. Here is the code of the function ( I also tried using the commented code) :
typedef void (*AppFunction)(void);
void JumpToApplication(void) {
AppFunction appEntryPoint = (AppFunction)APP_START_ADDRESS;
//__disable_irq();
//SCB->VTOR = APP_START_ADDRESS;
appEntryPoint();
}
Nothing is working and I don´t know what I am doing wrong