Bootloader UART Issue – STM32G070CBT6 (DFU Works, but No Response via UART)
Hello ST team,
I am experiencing an issue when trying to access the bootloader via UART on the STM32G070CBT6 and STM32L4R5ZI microcontrollers. When I set BOOT0 = 1, the bootloader works correctly via DFU (USB), but no response is received from the UART interface.
Tests Performed:
Bootloader Activation via Hardware (BOOT0 = 1):
- When I set BOOT0 = 1 and reset the microcontroller, it successfully enters DFU mode, and it is recognized by STM32CubeProgrammer via USB.
- However, none of the UART interfaces respond to the 0x7F (Get) command.
Testing Different UART Interfaces:
- I tested USART1, USART2, and USART3 on both microcontrollers.
- None of the UART ports respond to the bootloader protocol.
- Important: I verified the UART communication using an Arduino as a USB-UART converter and a custom software to send and receive data via UART. The UART communication works correctly in this scenario, confirming that the microcontroller's hardware and serial connection are operational.
Reading Bootloader Registers:
- I developed a software tool to read and modify the registers related to the bootloader (BOOT_SELECT, nBOOT0, etc.).
- The register values confirm that the settings are being correctly applied and that the System Boot memory is being activated.
Serial Communication Configuration:
- Tested multiple baud rates: 9600, 115200, 57600, 38400.
- Used STM32CubeProgrammer, minicom, picocom, and screen on Linux.
- No response to the 0x7F command, and STM32CubeProgrammer returns a timeout error when attempting to connect via UART.
Readout Protection (RDP) Check:
- RDP is set to Level 0 (0xAA), ensuring that the bootloader is accessible.
Questions:
- Does the bootloader in these models support UART for firmware programming, or only DFU via USB?
- Is there any additional configuration required to activate UART communication in the bootloader?
- Are there any known limitations in the STM32G070CBT6 and STM32L4R5ZI that could prevent the bootloader from working via UART?
I appreciate your assistance and look forward to your guidance on how to proceed.
Best regards