Bootloader (USB) DFU Issues on the new STM32G0B1xx
I had a previous issue with the generated CubeMX code, but saw it was already found in:
As per this fix, I am able to get USB DFU working in user flash. However, once connected in bootloader mode the device is not recognized, and in Windows I get a Device Descriptor Request Failed. This is the same error I got without the aforementioned fix in user flash.
PS: As of now I don't expect any hardware issues, as the STM32G0B1 connections are very straightforward, and I was able to get the USB working in user flash.
PPS: Previous issues I found on the community are not relevant to this MCU, as this has all the hardware for USB already built in. The reference manual and datasheet also confirm that the internal clock should be sufficient.