BUG AZRTOS NetXDuo v6.4 netx-duo-dhcpv6-client function nx_dhcpv6_request_solicit()
According to manual below, function should SEND out a SOLICIT message.
Function returns NX_SUCCESS (0x00) means SOLICIT message successfully sent.
Actually code, after some checks, just set nx_dhcpv6_state variable in DHCPv6 to NX_DHCPV6_STATE_SENDING_SOLICIT value and returns ALWAYS NX_SUCCESS, regardless of what DHCPv6 thread will do.
Therefore we will get NX_SUCCESS before actual sending the SOLICIT packet and even if this packet is not sent at all by DHCPv6 thread for any reason, e.g. no packets available in packet pool.
Also very critical, there is no high level function that user can use yo check for status end errors in DHCPv6 thread, no way to implement correctives actions unless to access global variables and void any quality certification.
nx_dhcpv6_request_solicit
Send a SOLICIT message
Prototype
UINT nx_dhcpv6_request_solicit(NX_DHCPV6 *dhcpv6_ptr);
Description
This service sends a SOLICIT message out on the network. If the message is successfully sent, a successful status is returned. A successful completion does not mean the Client received a response or has been granted an IPv6 address yet. The DHCPv6 Client thread task waits for a reply (an ADVERTISE message) from a DHCPv6 Server. If one is received, it checks the reply is valid, stores the data to the Client record and promotes the Client to the REQUEST state.
Note: If the Rapid Commit option is set, the DHCPv6 Client will go directly to the Bound state if it receives a valid Server ADVERTISE message. See the service description for nx_dhcpv6_request_solicit_rapid for more details.
Input Parameters
dhcpv6_ptr: Pointer to DHCPv6 Client instance
Return Values
NX_SUCCESS (0x00) SOLICIT message successfully sent
NX_PTR_ERROR (0x16) Invalid pointer input
NX_CALLER_ERROR (0x11) Must be called from thread
Allowed From
Threads