Bug in stm32h7rsxx_hal_cortex.c -- MPU regions are never enabled
The net effect of this bug is that the reference code (including the Templates for LRUN and XIP) never actually enable the Memory Protection Unit regions.
See: stm32h7rsxx_hal_cortex.c Line 532
I believe the second "Disable the Region" should have been an "Enable the Region", and called SET_BIT(MPU->RASR, MPU_RASR_ENABLE_Msk).
Without this, the result after a call to HAL_MPU_ConfigRegion is a disabled region, requiring a second call to HAL_MPU_EnableRegion(). Note that there are no calls to this function in the H7RS reference code or templates. As a result, these regions are never enabled.
I discovered this issue when a region I marked as non-cachable was being cached despite the region specifically declaring it as NOT_CACHABLE.