Solved
Bug report: Incorrect validation in com port initalization of nucleo (G4) BSP
When using the register callbacks feature ( USE_HAL_UART_REGISTER_CALLBACKS = 1) , the BSP does not register the default callback, causing the serial port not to work.
Fix:
diff --git a/Drivers/BSP/STM32G4xx_Nucleo/stm32g4xx_nucleo.c b/Drivers/BSP/STM32G4xx_Nucleo/stm32g4xx_nucleo.c
index 89b0837..bd2dd97 100644
--- a/Drivers/BSP/STM32G4xx_Nucleo/stm32g4xx_nucleo.c
+++ b/Drivers/BSP/STM32G4xx_Nucleo/stm32g4xx_nucleo.c
@@ -384,7 +384,7 @@ int32_t BSP_COM_Init(COM_TypeDef COM, COM_InitTypeDef *COM_Init)
/* Init the UART Msp */
COM1_MspInit(&hcom_uart[COM]);
#else
- if(IsComMspCbValid == 0U)
+ if(IsComMspCbValid[COM] == 0U)
{
if(BSP_COM_RegisterDefaultMspCallbacks(COM) != BSP_ERROR_NONE)
{