Bug STM32F429ZI ETH PTP TIM2 ITR1
STM32Cube FW_F4 V1.27.1
HAL ETH PTP
file
stm32f4xx_hal_tim_ex.c
Definition of TIM_TIM2_ETH_PTP
line 75-79
#if defined(TIM8)
#define TIM_TIM2_TIM8_TRGO 0x00000000U /*!< TIM2 ITR1 is connected to TIM8 TRGO */
#else
#define TIM_TIM2_ETH_PTP TIM_OR_ITR1_RMP_0 /*!< TIM2 ITR1 is connected to PTP trigger output */
#endif /* TIM8 */
fix:
#if defined (TIM2)
#if defined(TIM8)
#define TIM_TIM2_TIM8_TRGO 0x00000000U /*!< TIM2 ITR1 is connected to TIM8 TRGO */
#endif /* TIM8 */
#define TIM_TIM2_ETH_PTP TIM_OR_ITR1_RMP_0 /*!< TIM2 ITR1 is connected to PTP trigger output */