Skip to main content
Graduate
September 16, 2025
Question

Bug suspected in .h with repercussions on HAL for STM32G4 (RNG macros)

  • September 16, 2025
  • 1 reply
  • 270 views

Hi,

I discovered today with some of my students this potential bug in the stm32g431xx.h file:

 

#define RNG_CR_CED_Pos (5U)
#define RNG_CR_CED_Msk (0x1UL << RNG_CR_IE_Pos) /*!< 0x00000020 */
#define RNG_CR_CED RNG_CR_IE_Msk

As RNG_CR_IE_Pos is equal to 3... This mask is not correct.

It is quite strange: the comment is true... according to the Reference manuel 0440.

I suggest this correction:

 

#define RNG_CR_CED_Pos (5U)
#define RNG_CR_CED_Msk (0x1UL << RNG_CR_CED_Pos) /*!< 0x00000020 */
#define RNG_CR_CED RNG_CR_CED_Msk

 

 

(I checked the last version of this file using this official github : https://github.com/STMicroelectronics/cmsis-device-g4/blob/7c39c32593b03764aaa57531588b8bf7cdd443a5/Include/stm32g431xx.h )

 

In the HAL, the assert can't detect the fail... "checking itself" : 

assert_param(IS_RNG_CED(hrng->Init.ClockErrorDetection));

And this line used this CED... faking:

MODIFY_REG(hrng->Instance->CR, RNG_CR_CED, hrng->Init.ClockErrorDetection);

've fun...

Thx,

Samuel.

 

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    September 16, 2025

    Hello @samuel23 

    Thank you for bringing this issue to our attention.

    I reported this internally.

    Internal ticket number: 217616 (This is an internal tracking number and is not accessible or usable by customers).