Build error in CubeIDE. fatal error: lwipopts.h: No such file or directory
Hi
I cannot understand why my opt.h file cannot see the lwipopts.h file in the same folder.
Presumably, it must be something to do with the 'Wno-stringop-overflow' warning.
This contains a very long string -
-mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32H743xxDUSE_STM32H7XX_NUCLEO_144_MB1364 -c -I../../../Src -I"D:/halfcontainer/projects/cubeideN/LwIP_HTTP_Server_Netconn_RTOS/SW4STM32/STM32H743ZI_Nucleo/Middlewares/LwIP" -I../../../Drivers.......+ about 200 chars-
Can anyone tell me how to find out whats happening?
Trying to look back at sys_arch.c is a bit frightening! (To me at least)
Thanks,
Chris
18:12:19 **** Incremental Build of configuration Debug for project LwIP_HTTP_Server_Netconn_RTOS ****
make all
arm-none-eabi-gcc -Wno-stringop-overflow "../Middlewares/Third_Party/LwIP/system/OS/sys_arch.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32H743xx -DUSE_STM32H7XX_NUCLEO_144_MB1364 -c -I../../../Src -I"D:/halfcontainer/projects/cubeideN/LwIP_HTTP_Server_Netconn_RTOS/SW4STM32/STM32H743ZI_Nucleo/Middlewares/LwIP" -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H7xx_Nucleo -I../../../Drivers/BSP/Components/Common -I../../../Drivers/BSP/Components -I../../../Middlewares/Third_Party/LwIP/src/include -I../../../Middlewares/Third_Party/LwIP/system -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../../../Middlewares/Third_Party/FreeRTOS/Source -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Utilities -I../../../Drivers/CMSIS/Include -Os -ffunction-sections -Wall -fstack-usage -MMD -MP -MF"Middlewares/Third_Party/LwIP/system/OS/sys_arch.d" -MT"Middlewares/Third_Party/LwIP/system/OS/sys_arch.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Middlewares/Third_Party/LwIP/system/OS/sys_arch.o"
In file included from ../../../Middlewares/Third_Party/LwIP/src/include/lwip/debug.h:41,
from ../Middlewares/Third_Party/LwIP/system/OS/sys_arch.c:34:
../../../Middlewares/Third_Party/LwIP/src/include/lwip/opt.h:51:10: fatal error: lwipopts.h: No such file or directory
51 | #include "lwipopts.h"
| ^~~~~~~~~~~~
compilation terminated.
make: *** [Middlewares/Third_Party/LwIP/system/OS/subdir.mk:19: Middlewares/Third_Party/LwIP/system/OS/sys_arch.o] Error 1
"make all" terminated with exit code 2. Build might be incomplete.
18:12:25 Build Failed. 2 errors, 0 warnings. (took 5s.573ms)