C-Library const-correctness for STM32F1xx
I think const-correctness is an important-enough concept to call this a bug report.
In the HAL Driver for STM32F1xx, much of the codebase is not const-correct. For G4xx, I see that I2C is not.
What is const-correctness in C?
If a function that accepts a pointer to some data doesn't change that data, the function can tell the calling context that fact by declaring the buffer pointer to be const, like so:
void i_do_not_change_the_data(const void * data_ptr);
Then the calling context can be sure that the function will not attempt to write to the buffer, and can take advantage of compiler and language optimizations surrounding const arguments. One such (poor) example is a string literal, which can serve as a const char * argument, but not a char * argument.
Most (all?) of the HAL functions that take pointers to buffers take non-const pointers, even if those functions don't write to the buffer. That means that I cannot write my own code to be const-correct without casting away the constness, exposing my code to undefined behaviors.
Unfortunately, this problem runs extremely deeply in the library code, all the way down to HAL struct members. TX buffers in particular should be declared as const *, but they're not, so const pointers can't be assigned to them and the APIs can't be corrected.
This needs an intense application of effort to correct. If ST intends its HAL libraries to be suitable for production code, this really ought to be fixed.
All pointer arguments to functions should be const unless they can't be. Const-ness should be a forethought, not an afterthought.