Can I communicate with high speed device using Full speed host(NUCLEO-F411RE)?
I am working on USB CDC ACM device. I want to communicate with High Speed device using full speed host(NUCLEO-F411RE). As I am new to USB protocol, but I know that device starts communication in FS mode and switch to HS mode only if host respond to J-K chirp signal.
- Device is enumerated and detected as full speed device.
- Descriptor is successfully received on host
- It is high speed device but detected as FS to my host. Bulk endpoint(IN and OUT) size of device is 512 Bytes.
- Device transmits data when I send specific character to device, I transmit that data from host and host receive ACK from device.
- After that I am waiting for data from device, but I don't get any data.
- I am suspecting that it might be due to Bulk Endpoint size.
When I am communication between two STM32 NUCLEO-F411RE board one as HOST and other as DEVICE then data is transmitted and received successfully.
When device is connected with PC(host) I am able to get reply from device.
IDE used : STM32CubeIDE