Skip to main content
Super User
June 11, 2025
Question

Can LL_GPIO_Init() initialize multiple pins at once?

  • June 11, 2025
  • 2 replies
  • 505 views

In an inherited code I see LL_GPIO_Init() being called with pin definitions (LL_GPIO_PIN_xx) OR-ed together, presumably to define multiple pins of the same port to the same settings, in one call of the function.

The documentation (doxygen header) to LL_GPIO_Init() does not say this is allowed; neither says so the description of the init struct. Is there any authoritative documentation which allows this?

Thanks,

JW

 

    This topic has been closed for replies.

    2 replies

    Super User
    June 11, 2025

    I've always found this to be unclear in both HAL and LL documentation.

    It's never clear whether a "pin" parameter represents a pin number (so can only be a single pin), or a bitmask (so could represent multiple pins) - and both are used in various places.

     

    PS:

    See: https://community.st.com/t5/stm32-mcus-embedded-software/array-for-gpio-pins/m-p/654354/highlight/true#M46755

    But the documentation:

    AndrewNeil_0-1749633364422.png

    Is not at all clear that GPIO_Pin is a bitmask.

    Super User
    June 11, 2025

    In this case, neither of them, LL_GPIO_PIN_xx definitions contain multiple (three?) fields, neither of them is pin number and only one of them is the pin mask.

    Nonetheless, LL_GPIO_Init() as it is now *is* written with the multiple-pins-at-once in mind; however, I am hesitant to rely on that once there's not a single iota hinting toward this option in the documentation I know of.

    JW

    Super User
    June 11, 2025

    I think those definitions do boil down to a bitmask for each pin:

    /** @defgroup GPIO_LL_EC_PIN PIN
     * @{
     */
    #define LL_GPIO_PIN_0 ((GPIO_BSRR_BS0 << GPIO_PIN_MASK_POS) | 0x00000001U) /*!< Select pin 0 */
    #define LL_GPIO_PIN_1 ((GPIO_BSRR_BS1 << GPIO_PIN_MASK_POS) | 0x00000002U) /*!< Select pin 1 */
    #define LL_GPIO_PIN_2 ((GPIO_BSRR_BS2 << GPIO_PIN_MASK_POS) | 0x00000004U) /*!< Select pin 2 */
    #define LL_GPIO_PIN_3 ((GPIO_BSRR_BS3 << GPIO_PIN_MASK_POS) | 0x00000008U) /*!< Select pin 3 */

     

    Especially given the final "ALL" definition:

    #define LL_GPIO_PIN_ALL (LL_GPIO_PIN_0 | LL_GPIO_PIN_1 | LL_GPIO_PIN_2 | \
     LL_GPIO_PIN_3 | LL_GPIO_PIN_4 | LL_GPIO_PIN_5 | \
     LL_GPIO_PIN_6 | LL_GPIO_PIN_7 | LL_GPIO_PIN_8 | \
     LL_GPIO_PIN_9 | LL_GPIO_PIN_10 | LL_GPIO_PIN_11 | \
     LL_GPIO_PIN_12 | LL_GPIO_PIN_13 | LL_GPIO_PIN_14 | \
     LL_GPIO_PIN_15) /*!< Select all pins */

     

    But, indeed, this still doesn't guarantee that any particular function/macro taking them as a parameter will actually work with a multi-pin pattern.

     

    So, indeed, this documentation needs to be clarified.

    Throughout.

    Super User
    June 11, 2025

    > I think those definitions do boil down to a bitmask for each pin

    Only bits 8..24 are the actual pin mask, filled by (GPIO_BSRR_BSx << GPIO_PIN_MASK_POS)

    Bits 0..7 (which in itself wouldn't be sufficient for a mask for all 16 pins) is something like "(half of) shift within one of the CRL/CRH registers" (this is 'F1, very different from other STM32; but in other STM32 that 8-bit mask is "shift wihin one of the ARL/ARH registers).

    Then there's a flag somewhere at 26th bit which probably is "index" distinguishing between CRL/CRH. I am not going to dig deeper.

    > Especially given the final "ALL" definition

    The only purpose of the "ALL" is to be used in the "checker" macro, where it verifies that at least one of those 3 fields is nonzero and all other bits not occupied by those fileds are zero.

     

    The HAL_GPIO_WritePin() you've quoted above *is* different from the initialization and it may indeed require only one pin at a time (not going to dig into that either).

    JW