Can't enumerate USB with STM32F44RE (custom board)
I am trying to setup USB communication with an STM32F446RE
It is a custom board where:
- The clock source is an external 8Mhz quartz
- There is a micro USB port with USB+ connected to PA12 and USB- connected to PA11
The external quartz is working (I can load a firmware that just blinks a led) but I fail to enumerate the USB device with below message in the computer syslog.
I am using mbed with the NUCLEO F446RE configuration, I just enabled USB in the target configuration (USE_USB_OTG_FS type)
Also, I noted that if I plug the board even without a firmware that is supposed to use USB, my computer tries to enumerate the device, however it shows a different message (like it's trying to enumerate a low-speed device instead of high-speed)
Do you have any idea/clue what could be going wrong?
Oct 23 19:13:51 destiny kernel: [4213209.733361] usb 1-10: new full-speed USB device number 17 using xhci_hcd
Oct 23 19:13:51 destiny kernel: [4213209.861500] usb 1-10: device descriptor read/64, error -71
Oct 23 19:13:51 destiny kernel: [4213210.097415] usb 1-10: device descriptor read/64, error -71
Oct 23 19:13:51 destiny kernel: [4213210.333311] usb 1-10: new full-speed USB device number 18 using xhci_hcd
Oct 23 19:13:51 destiny kernel: [4213210.461545] usb 1-10: device descriptor read/64, error -71
Oct 23 19:13:52 destiny kernel: [4213210.697528] usb 1-10: device descriptor read/64, error -71
Oct 23 19:13:52 destiny kernel: [4213210.805438] usb usb1-port10: attempt power cycle
Oct 23 19:13:52 destiny kernel: [4213211.461355] usb 1-10: new full-speed USB device number 19 using xhci_hcd
Oct 23 19:13:52 destiny kernel: [4213211.461721] usb 1-10: Device not responding to setup address.
Oct 23 19:13:53 destiny kernel: [4213211.669583] usb 1-10: Device not responding to setup address.
Oct 23 19:13:53 destiny kernel: [4213211.877357] usb 1-10: device not accepting address 19, error -71
Oct 23 19:13:53 destiny kernel: [4213212.005324] usb 1-10: new full-speed USB device number 20 using xhci_hcd
Oct 23 19:13:53 destiny kernel: [4213212.005568] usb 1-10: Device not responding to setup address.
Oct 23 19:13:53 destiny kernel: [4213212.213745] usb 1-10: Device not responding to setup address.
Oct 23 19:13:53 destiny kernel: [4213212.421346] usb 1-10: device not accepting address 20, error -71
Oct 23 19:13:53 destiny kernel: [4213212.421442] usb usb1-port10: unable to enumerate USB device