Can't ping between Windows and Linux CDC ECM - Ethernet
Hi, I have a problem with pinging PCs with my adapter USB-Ethernet with an STM32F207. I'm currently working with CDC-ECM for Ethernet-Over-USB.
First case: I have 2 VMs with Linux on them. The USB is connected to the first VM (VM1) and the Ethernet is connected to the second (VM2). I can ping VM1 with VM2 but I can't ping VM2 with VM1.
Second case: I have one VM with Linux and a Windows machine. The USB is connected to the VM and the ethernet is connected to the Windows machine. When I ping the VM with Windows or Windows with the VM I have only loss packets...
Does someone have any idea why ?
Thanks,