Can the STUSB4761 as a standalone device perform a DR_Swap?
We have an application that's currently using a USB BC1.2 IC to enumerate a charge condition (CDP) between a USB-u sinking host and a sourcing device. We're looking to add an IC between the existing circuit acting as the sourcing device and a USB-C device that would allow for the USB-C device to become the sinking DFP. If the USB-C peripheral starts out as a sinking UFP and initiates a DR_SWAP command, will the STUSB4761 be able to complete the sequence for the data role swap and allow the USB-C peripheral to act as a sinking DFP? Can this be done with only the STUSB4761, without the need for any other external memory, MUX, etc?