Skip to main content
Explorer
January 9, 2025
Solved

Cannot Extract STSW-SAFEA1-MW

  • January 9, 2025
  • 1 reply
  • 460 views

Hi,

I am having trouble extracting the STSW-SAFEA1-MW. This is the same issue mentioned here and here. I can't use your product if I can't use your drivers. A fix would be appreciated.

Thanks

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Welcome @rlederhose, to the community!

    I also tested this again after @Frantz LEFRERE tried it here and also had problems with some unzip programmes. However, the ZIP can be unpacked very well with the open source (un)packer 7-z.

    Hope that helps?

    Regards
    /Peter

    1 reply

    Technical Moderator
    January 9, 2025

    Welcome @rlederhose, to the community!

    I also tested this again after @Frantz LEFRERE tried it here and also had problems with some unzip programmes. However, the ZIP can be unpacked very well with the open source (un)packer 7-z.

    Hope that helps?

    Regards
    /Peter

    Explorer
    January 9, 2025

    Thanks for the help Peter! 7zip worked a treat.