Skip to main content
Visitor II
September 19, 2020
Question

Cannot see USB_FS on STM32F373VCT6 as VCP.

  • September 19, 2020
  • 0 replies
  • 520 views

Hi I have STM32F373VCT6 on the board that I am bringing up. I am trying to open up the USB_FS as VCP. I use 20 MHz oscillator, which gives 48 Mhz USB clock and 24 MHz for APB2. I use the code below:

 while (1)

 {

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

CDC_Transmit_FS(myBuf, 4);

HAL_Delay(1000);

 }

This code when I target to an EVK based on STM32H750VIB-dK works fine and I could see the VCP. The hardware is missing the transient suppressor but the rest seems fine, including the differential pair. The USB_FS signals go to PA12 (usb_dp) and PA11 (usb_dm). Part of the schematic is below. Can anyoe help? Thanks

    This topic has been closed for replies.