Change SPI speed (clock prescaler) and resume operation on H7
Hello,
I'd like to change speed (clock prescaler setting in CFG1) and then resume sending bytes on SPI.
Right now, I do :
retval = HAL_SPI_Abort(&hspi2);
My_SPI2_Init(SPI_EyeGenPrescaler);where My_SPI2_Init is just slightly customized version of Mx_SPI2_Init with new Prescaler value as input argument.
After this, I don't see anything on SPI MOSI output.
What am I doing wrong? Is something else needed to shutdown SPI and initialize it at new prescaler value ?
Can I somehow change speed more fine-grained than just changing prescaler to values like powers of 2 ?
Thanks,
regards.