Changing default memory sections
I'm working on some code that has a boot loader and an application. At the moment I am using one linker script for each, which means I have to make sure I keep them in sync. Is it possible to configure the build for (e.g.) the boot loader so that .boottext is used instead of .text for the code so that a single linker file can be used?
I've tried searching (here and internet) and it appears as if this can't be done with GCC - but I thought it was worth asking just in case I've missed something.