COMP triggered ADC too slow
Hi,
1. [Part Number] NUCLEO-L432KC
2. [Environment] STM32CubeIDE 1.14.1
3. [Schematics] NA
4. [Details] I am trying to measure a fast pulse with the ADC (~3 us rise time). I would like to trip a comparator when the pulse starts to rise and then start an ADC (paced by a timer) to fill a buffer via DMA. After the buffer is full, I will send the data over UART for analysis.
The COMP and ADC are both connected to the same input. The COMP is set to trigger when the voltage exceeds that of an external input set to 0.04 volts. The ADC is connected to a timer that triggers at 2 Mhz.
I wait for HAL_COMP_TriggerCallback and then start the ADC with DMA:
void HAL_COMP_TriggerCallback(COMP_HandleTypeDef *hcomp) {
if (hcomp == &hcomp1)
{
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)voltage_buf, VOLTAGE_BUF_LEN);
HAL_COMP_Stop_IT(&hcomp1);
}
}
5. [Problem and Expected behavior] I have configured the above but I am seeing that the first ADC reading starts well after the pulse has started. Should I expect the time to start the ADC from a COMP to be this slow? I would like to measure the peak voltage which means that I need to capture at least some of the rising edge of the pulse.
6. [How to reproduce] I have attached the project files. Please see the attached oscilloscope view of the pulse and the plot of the ADC buffer values.


7. [Occurrence]
8. [Sanity checks] Removed all blocking code in the interrupt callback to try to speed up. Googled around for "slow comparator start-up".