Comparator with PWM
In my setup, I’m using Comparator 6 (COMP6) on the STM32G474 microcontroller. The non-inverting input of the comparator is connected to a burden resistor from a current transformer, which measures current flow. The inverting input is tied to a fixed 1.5V reference created by a voltage divider. The goal is for the comparator to disable all PWM signals (generated by HRTIM TimerA) when the burden resistor voltage reaches 1.5V, indicating an overcurrent condition (e.g., 10A).
Issue: Despite the burden resistor voltage hitting 1.5V at 10A, the comparator does not trigger, and the PWM remains active.