Compilation Error Due to stm32h5xx_util_i3c.h Missing USE_FULL_LL_DRIVER Flag Protection
In the STM32H5 HAL, the file stm32h5xx_util_i3c.h was not included in the compilation list because it does not contain protection with the #if defined (USE_FULL_LL_DRIVER) flag, even though it uses the LL driver. This absence of protection results in a compilation error when the USE_FULL_LL_DRIVER flag is not defined.
Steps to Reproduce:
- Attempt to compile a project that references stm32h5xx_util_i3c.h without defining USE_FULL_LL_DRIVER.
- Observe the compilation failure due to missing flag protection in the file.
Suggested Solution:
Add conditional compilation protection around the code in stm32h5xx_util_i3c.h using #if defined (USE_FULL_LL_DRIVER). This would prevent compilation issues when the full LL driver is not in use.