configuration of stm32f407(SAI/i2s)
hello,
I am using Stm32f407 with an IM69D120 mic. I have couple of questions regarding the interface and configuration of the mic.
1) Is it possible to configure the audio codec with a 4 kHz sampling frequency and a 16-bit resolution?
2) Which interface should I use for configuration: i2S or SAI? (Which interface gives more control while configuring the clock and OSR?)
Regards,
Manikandan V