Confusion about length parameter in HAL_TIM_PWM_Start_DMA
Hi,
I have NUCLEO-F411RE and NUCLEO-U575ZI-Q boards. When trying to implement a sine curve with PWM and a low-pass filter I stumbled into problems with HAL_TIM_PWM_Start_DMA.
I store the precomputed sine data in an array and call HAL_TIM_PWM_Start_DMA.
... BEGIN: pseudo code
uint16_t pwmData[PWM_SAMPLES];
compute_sine_data(pwmData);
HAL_TIM_PWM_Start_DMA(&htimX, TIM_CHANNEL_1, (uint32_t *) pwmData, PWM_SAMPLES);
... END: pseudo code
It works fine on STM32F4, but I noticed only half of the data is present on the STMU575. Apparently HAL_TIM_PWM_Start_DMA has different semantics on the 2 MCUs. On STM32F4 the length seems to be with respect to Data Width in the timers DMA setting, and on STM32U575 it seems to be measured in bytes (regardless of the GPDMA settings).
In short:
STM32F4: HAL_TIM_PWM_Start_DMA(&htimX, TIM_CHANNEL_1, (uint32_t *) pwmData, PWM_SAMPLES);
STM32U5: HAL_TIM_PWM_Start_DMA(&htimX, TIM_CHANNEL_1, (uint32_t *) pwmData, 2*PWM_SAMPLES);
I noticed that HAL_TIM_PWM_Start_DMA is calling HAL_DMA_Start_IT on STM32F4 and TIM_DMA_Start_IT on STM32U5.
So is this behavior a bug or a feature?