Skip to main content
Visitor II
February 21, 2025
Question

Connect to the multiple Cellular hardware

  • February 21, 2025
  • 1 reply
  • 574 views

I'm working on an STM32 project using X-CUBE-CELLULAR to support both cellular modems: BG96 (or GM01Q). I physically connected both modems (2× STMod+ expansion connectors) to my STM32 board.

My main question is: How can I configure my project and steps to allow me to select and switch between controlling either the BG96 or the GM01Q modem at runtime using the X-CUBE-CELLULAR package?
If the package already supported, which configuration we should attend ?

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    March 28, 2025

    Hello @Alan5 

    I reported your question internally and will get back to you as soon as possible.

    Internal ticket number: 206379 (This is an internal tracking number and is not accessible or usable by customers).