Connect with LwIP to port 5000
Hi Guys,
I want to connect a server via port 5000.
When connecting to other server with port 80 there is no problem, but when connecting with port 5000 it doesn't works.
IP_ADDR4( &remote_ip, 11, 12, 13, 14);
CommDropsTcpConn = netconn_new(NETCONN_TCP);
netconn_connect(CommDropsTcpConn, &remote_ip, 5000); --> return -14 (ERR_RST)
what do I need to configure to support connection to port 5000,? (or any port other than 80..)
Thanks,
Lior