Skip to main content
Graduate
July 8, 2025
Solved

Creating HID keyboard using USBX

  • July 8, 2025
  • 3 replies
  • 483 views

I'm trying to generate an HID keyboard through CubeMX for USBX. I'm using an F411CE based board so picked the appropriate software pack for that. However, when I go to pick to pick components, I can only see the generic HID pack instead of separate keyboard and mouse packs as I've seen here before. I'd usually be fine with this and add the keyboard files in myself but this generic HID pack is based on a mouse implementation and adds a lot of unnecessary bloat to the stack. Is there a way to generate the files without the ux_device_mouse files?

    This topic has been closed for replies.
    Best answer by FBL

    Hi @mahirmahota 

    X-Cube-Azrtos-F4 is an old pack. You might find some differences in CubeMX implementation.

    An internal ticket is submitted to dedicated team to separate USBX components in code generation (214068).

    3 replies

    FBLAnswer
    Technical Moderator
    July 14, 2025

    Hi @mahirmahota 

    X-Cube-Azrtos-F4 is an old pack. You might find some differences in CubeMX implementation.

    An internal ticket is submitted to dedicated team to separate USBX components in code generation (214068).

    Graduate
    July 15, 2025

    Hi!

    I'd prefer to use USBX since I'm implementing ThreadX for the rest of my application. Is the RTOS implementation outdated after Microsoft ended support and is the classic USB class back to being the preferred method of doing this now?

    Graduate II
    July 16, 2025

    Understood and good question. I was wondering myself if STM were going to rework all the ThreadX examples with FreeRTOS. It's definitely an about-face.

    Technical Moderator
    July 17, 2025

    Hello @mahirmahota @Grant Bt 

    You might need to look at this threadSoon, we will provide example using FreeRTOS as the main kernel, integrating it with USBX.