Creating new Project with X-CUBE-AUDIO-KIT
I am working on an audio application which is to be built on a custom board using STM32H723VG and the X-CUBE-AUDIO-KIT V1.1.1. I have demonstrated a prototype solution using the pre-built AUDIO-KIT binary loaded on the STM32H735G-DK development board and running LiveTune. I would now like to use AUDIO-KIT and create the similar real application for my target board with STM32H723VG.
Being relatively new to the STM32CubeIDE (Version 1.16.00) environment I am unclear how to create a new project using the AUDIO-KIT as a foundation and then altering the BSP for my implementation of the H723. Can someone please point me to documentation or provide assistance for this?