CubeIDE fatal error: stm32h7xx_hal.h: No such file or directory
Apologies - posted to wrong forum group
Host: amd64, 8GB RAM, 500GB SSD, 440GB available
Ubuntu 20.04, all current updates
Installed the debian amd64 1.11.2 CubeIDE and 6.7.0 MX.
Created a simple H750V application using MX. The IDE installed the
current HAL H7xx library. Building the bare bones before adding more
application code produced the fatal error for the line 36 #include
statement in stm32h7xx_hal.c, plus many syntax error warnings in
stm32h7xx.c, such as in line 71 __IO uint32_t uwTick;.
I did not modify stm32h7xx_hal_conf.h file.
In case files were somehow corrupted, replaced the IDE loaded files stm32h7xx_hal.h and stm32h7xx_hal.c with files from a 1.11.0 HAL separately downloaded HAL library. The same errors ocurred.
ioc file is attached.
Cheers, Hal