Skip to main content
Visitor II
September 26, 2025
Question

Custom Bootloader Integration on STM32H747IIT6 for FOTA Application

  • September 26, 2025
  • 1 reply
  • 845 views

Dear ST Community/Support Team,

 

We are developing a Firmware Over-The-Air (FOTA) solution for an IoT asset tracking device using the STM32H747IIT6 microcontroller (LQFP176 package, dual-core Cortex-M7/M4, 2MB dual-bank Flash). The system integrates a SIMCOM cellular/GNSS module for connectivity and location services, with firmware downloads staged via AT commands (e.g., HTTP for files like fwv1.bin) and processed using STM32 HAL UART/Flash APIs.

Project Overview:

  • Hardware: STM32H747IIT6 as main MCU; SIMCOM module on UART1 for AT commands (e.g., AT+FSOPEN/FSREAD for file staging); GNSS NMEA parsing on UART2 (offloaded to M4 core).
  • Software Stack: STM32CubeH7 HAL (v1.13+), FreeRTOS on M7 for multitasking, dual-bank Flash for safe updates (Bank1: Bootloader + Active App; Bank2: New Firmware).
  • FOTA Flow:
    • Poll server for update manifest (version, URL, checksum).
    • Download chunks to SIMCOM FS or SD card.
    • Verify (CRC/SHA256), copy to inactive bank, set flag, reset.
    • Bootloader validates and swaps banks on boot.
  • Current Progress: We have working app code for download (using custom SendAT and read_http_chunk functions) and GNSS position acquisition. Dual-core IPC via HSEM is set up.

Specific Request: Bootloader Integration Assistance We need technical guidance to implement and integrate a custom bootloader for seamless FOTA on the STM32H747IIT6. Key challenges include:

  • Dual-Bank Flash Management: Configuring option bytes for dual-bank mode (via CubeMX/STM32CubeProgrammer); handling bank swap (HAL_FLASHEx_OBProgram) without bricking; vector table relocation for Bank2 app.
  • Bootloader Structure:
    • Size: ~32-64KB in Bank1 start (address 0x08000000).
    • Features: CRC/signature verification of active app; check update flag (e.g., in RTC backup register or Bank1 end); jump to app (modify VTOR, set MSP); optional GNSS query for geo-validation during boot.
    • No RTOS in bootloader (lean C/Assembly); use HAL Flash API for programming Bank2.
  • Integration with Application:
    • From app: Erase/program Bank2 (HAL_FLASHEx_Erase, HAL_FLASH_Program), set flag, call NVIC_SystemReset().
    • Post-Reset: Bootloader detects flag, swaps (option bytes), jumps to new app entry (e.g., 0x08100000 for Bank2).
    • Dual-Core Handling: Ensure M4 firmware is updated (copy to M4 Flash area); sync via RPC/HSEM.
  • Security and Reliability:
    • Basic secure boot (public key in OTP); handle partial updates/power loss (checkpointing).
    • Rollback: If new app fails (e.g., watchdog), revert to previous bank.
  • Tools/Environment: STM32CubeIDE 1.14+, CubeMX for code gen, Arm GCC compiler. We've enabled dual-bank in RCC/Flash settings but face issues with [briefly describe any specific errors, e.g., "option byte programming hangs" or "vector table misalignment after swap"].

What We Need Help With:

  • Sample code/skeleton for the bootloader (e.g., full .c/.s files for verification, swap, and jump).
  • Best practices for H747IIT6-specific pitfalls (e.g., cache invalidation during Flash ops, M7/M4 vector tables).
  • Troubleshooting: Common errors in dual-bank FOTA (e.g., HAL return codes, linker script mods for Bank2).
  • References: Beyond AN5347/UM2854, any H7-specific app notes or examples (e.g., from STM32CubeH7 repo).
  • If possible, a walkthrough or debug tips for testing on [our board, e.g., custom PCB or STM32H747IIT6.

Thank you for your expertise!

Best regards,
Rahul Temkar

    This topic has been closed for replies.

    1 reply

    ST Employee
    October 2, 2025

    Hello @rahuliotas 

    There is an OpenBootloader application in the STM32H7RS firmware package (available on GitHub) that can assist you. Additionally, AN2606 provides guidance for verifying the communication interface. You can also draw inspiration from the FUOTA applications deployed on the WL series, specifically the NUCLEO-WL55JC board: LoRaWAN_FUOTA and LoRaWAN_FUOTA_DualCore.

    With regards