Custom PCB, STM32H7 and KSZ8863RLL, RMII
Hi
I have made a custom PCB based on STM32H723VGT MCU and KSZ8863RLL with interface RMII. I have followed the Hardware Design Guide for the KSZ8863. Including 100 Ohm impedance from RJ45 to PHY and 50 Ohm impedance from PHY to STM32. Length matching is also done with meanders.
Without any configuration from CubeMx I am expecting some activity on the LEDS when I plug a ethernet cable in the RJ45 connector.
Are there anyone with experience with the KSZ8863 3-port switch, that have any suggestions? I have added a picture of the schematic. The crossed is not implemented on the board, so please ignore those.
Any help is much appreciated!
Friendly regards, David