Question
Data Corruption with USB CDC communication
Continuous transmission of data of tx rate 500 samples per seconds(33 bytes per sample) using USB virtual com port(USB CDC).
USB mode - full speed
Transmit data to serial monitor using function CDC_Transmit_FS();
Received data on serial monitor is corrupted data, and this data corruption is not regular.
To solve this problem -
- check the status of CDC_Transmit_FS() who check the state of variable(hcdc->TxState )
- send data after multiples of 1millisecond window.
- Set/reset flag continuous in CDC_TransmitCplt_FS() function.