Data transmited with I2C is garbled on STM32L476
Hello, I wanted to try I2C communication on my Nucleo board since I'm planning to use it in one of my designs. I connected together pins of I2C1 and I2C2, turned on internal pull-ups on both sides for all the pins and wanted to transmit "HELLO" from one to the other.


Code for transmitting:
HAL_I2C_Slave_Receive_IT(&hi2c1 ,(uint8_t *)RX_Buffer, 5);
status = HAL_I2C_Master_Transmit(&hi2c2, 72 << 1, *data, 5, 80000000);
After receiving the data however, even though status is set to HAL_OK it is completely garbled:

I looked at the signal waveforms on my osciloscope with the logic analyzer enabled, and it shows that it's exactly what was transmitted:

After that I thought that it might be an issue of the internal pull-ups not being strong enough, so I added 1K resistors on both data and clock lines, but the data in the receiving buffer is exactly the same. Does anybody know what am I doing wrong?