Debug the code through uart
Hi!
I am using STM32F373RCT6 controller on custom board. In that board we have used USB to serial convertere chip FT2232HL-REEL and it is connected to USART1 (PA9 and PA10).
STM32F373RCT6 system clock frequency is 70MHz.
Can I use USB to serial option to debug the code instead of ST Link V2? If Yes, how?
I want to flash the code through USB in our project.
If any other details required, please let me know.
Regards,
Gaurav