DFU driver (STTub30) causes a blue screen on windows 10?
Hi,
I'm using STM32L072KZT6 microcontroller, and I'm trying to make USB DFU Standalone bootloader. I've done many bootloader standalone firmwares for STM32 MCUs, for F0, F1, F3, F4 series, and had never encountered this kind of a problem. It's not deterministic, I've succeeded couple of times to write my firmware via DfuSe, and successfully run the main program, but in most cases it fails. Windows does not complain about the driver when the USB is plugged in, when I try to update it, it says that I'm already using the newest version.
The problem appears in the following moments:
- When USB is plugged in
- When Upgrade button is pressed inside DfuSe demo
I've tried different solutions, running DfuSe from STM32L folder, but nothing helped. My firmware is almost the same as an example for 32L0538DISCOVERY inside Cube L0 repository, and I'm using the latest version of L0 Cube firmware (V1.11.2). I've attached some pictures of the error message, driver version, and .zip file of my CubeIDE project.
Hope you can help me :)