Skip to main content
Visitor II
July 29, 2021
Solved

Differences between STM32F1 and STM32H7 series MCUs using USBX

  • July 29, 2021
  • 1 reply
  • 1057 views

I have successfully run the ThreadX+USBX program on the H7 chip. The USB composite device (CDC ACM+HID) is used, so I tried to implement the same function on F105RBT6, but I ran into trouble, running USB on F105 The composite device can run normally at the beginning, but after 30s, the USB will be disconnected and reconnected, and the USB will not be recognized. I learned that H7 has 9 endpoints and F1 has only 4 USB endpoints. Will it? Is USB working abnormally because of the number of endpoints?

    This topic has been closed for replies.
    Best answer by Walid ZRELLI

    Hello @arilink​ 

    Unfortunately, we have not planned to support STM32F1 devices until today.

    BeST Regards,

    Walid

    1 reply

    Visitor II
    August 2, 2021

    Hello @arilink​ 

    Unfortunately, we have not planned to support STM32F1 devices until today.

    BeST Regards,

    Walid