Difficulties with Writing to the Flash Memory of STM32L4R5
Hi,
I'm novice with the STM32 microcontrollers and this community.
I'm trying to write to the flash memory of STM32L4R5 in 'FLASH_TYPEPROGRAM_FAST' mode of the HAL_FLASH_Program().
The flash of the MCU is configured as Single Bank.
Writing to the flash only works when using 'FLASH_TYPEPROGRAM_DOUBLEWORD'. The flash reads as 0xFFFFFFFF when written in 'FLASH_TYPEPROGRAM_FAST' mode.
This is my test project:
// Page Erase Structure
static FLASH_EraseInitTypeDef EraseInitStruct;
// Page Erase Status
uint32_t eraseStatus;
// Data Buffer
uint64_t pDataBuf[32] =
{
0x1111111122222222, 0x3333333344444444,
0x5555555566666666, 0x7777777788888888,
0x12345678ABC12345, 0x23456789DEF01234,
0x34567890AAABBB12, 0x4567890FABCDDD34,
0x1111111122222222, 0x3333333344444444,
0x5555555566666666, 0x7777777788888888,
0x12345678ABC12345, 0x23456789DEF01234,
0x34567890AAABBB12, 0x4567890FABCDDD34,
0x1111111122222222, 0x3333333344444444,
0x5555555566666666, 0x7777777788888888,
0x12345678ABC12345, 0x23456789DEF01234,
0x34567890AAABBB12, 0x4567890FABCDDD34,
0x1111111122222222, 0x3333333344444444,
0x5555555566666666, 0x7777777788888888,
0x12345678ABC12345, 0x23456789DEF01234,
0x34567890AAABBB12, 0x4567890FABCDDD34
};
// Flash Page Start Address
uint32_t pageAddr = 0x081FE000;
// Fill Erase Init Structure
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Banks = FLASH_BANK_1;
EraseInitStruct.Page = 255;
EraseInitStruct.NbPages = 1;
// Unlocking the FLASH Control Register
HAL_FLASH_Unlock();
// Clear OPTVERR Bit Set on Virgin Samples
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
// Erasing the Flash Page
HAL_FLASHEx_Erase(&EraseInitStruct, &Error);
#if 0
// Wriring a Doubled Word to Flash. pDataBuf[0] is the 64-bit Word
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, pageAddr, pDataBuf[0]);
#else
// Wriring 32 Double Words. pDataBuf is the Starting Address of the 64-bit Array
HAL_FLASH_Program(FLASH_TYPEPROGRAM_FAST_AND_LAST, pageAddr, pDataBuf);
#endif
// Locking the FLASH Control Register
HAL_FLASH_Lock();Am I doing anything wrong?
Thank you,
Ivan