Displaying two animations simultaneously on ssd1306 oled display
Dear Sir/Madam,
Currently I am doing a project called "Displaying two animations simultaneously on ssd1306 oled display".
Problem :- For this I am using cmsis rtos v1 to create two separate tasks. One task handles one animation frames & the other task handles the other animation frames. But this is not achievable as expected.
So am I doing any mistakes?
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "cmsis_os.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "fonts.h"
#include "ssd1306.h"
#include "animation.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;
osThreadId Task1Handle;
osThreadId Task2Handle;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
void StartTask1(void const * argument);
void StartTask2(void const * argument);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
/* USER CODE BEGIN 2 */
SSD1306_Init();
SSD1306_GotoXY (0,0);
SSD1306_Puts ("SATYABRATA", &Font_11x18, 1);
SSD1306_GotoXY (0, 30);
SSD1306_Puts ("SENAPATI", &Font_11x18, 1);
SSD1306_UpdateScreen();
HAL_Delay (1000);
SSD1306_ScrollRight(0,7);
HAL_Delay(10000);
SSD1306_ScrollLeft(0,7);
HAL_Delay(10000);
SSD1306_Stopscroll();
/* USER CODE END 2 */
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
/* USER CODE END RTOS_MUTEX */
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
/* Create the thread(s) */
/* definition and creation of Task1 */
osThreadDef(Task1, StartTask1, osPriorityBelowNormal, 0, 128);
Task1Handle = osThreadCreate(osThread(Task1), NULL);
/* definition and creation of Task2 */
osThreadDef(Task2, StartTask2, osPriorityNormal, 0, 128);
Task2Handle = osThreadCreate(osThread(Task2), NULL);
/* USER CODE BEGIN RTOS_THREADS */
/* add threads, ... */
/* USER CODE END RTOS_THREADS */
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 84;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief I2C1 Initialization Function
* None
* @retval None
*/
static void MX_I2C1_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 400000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
/**
* @brief GPIO Initialization Function
* None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/* USER CODE BEGIN Header_StartTask1 */
/**
* @brief Function implementing the Task1 thread.
* argument: Not used
* @retval None
*/
/* USER CODE END Header_StartTask1 */
void StartTask1(void const * argument)
{
/* USER CODE BEGIN 5 */
/* Infinite loop */
for(;;)
{
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame1,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame2,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame3,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame4,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame5,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame6,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame7,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame8,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame9,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame10,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame11,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame12,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame13,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame14,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame15,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame16,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame17,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame18,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame19,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame20,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame21,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame22,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame23,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame24,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame25,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame26,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame27,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(60,0,animation_frame28,64,64,1);
SSD1306_UpdateScreen();
osDelay(1);
}
/* USER CODE END 5 */
}
/* USER CODE BEGIN Header_StartTask2 */
/**
* @brief Function implementing the Task2 thread.
* argument: Not used
* @retval None
*/
/* USER CODE END Header_StartTask2 */
void StartTask2(void const * argument)
{
/* USER CODE BEGIN StartTask2 */
/* Infinite loop */
for(;;)
{
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame1,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame2,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame3,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame4,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame5,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame6,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame7,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame8,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame9,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame10,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame11,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame12,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame13,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame14,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame15,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame16,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame17,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame18,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame19,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame20,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame21,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame22,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame23,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame24,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame25,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame26,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame27,64,64,1);
SSD1306_UpdateScreen();
SSD1306_Clear ();
SSD1306_DrawBitmap(0,0,weather_frame28,64,64,1);
SSD1306_UpdateScreen();
osDelay(1);
}
/* USER CODE END StartTask2 */
}
/**
* @brief Period elapsed callback in non blocking mode
* @note This function is called when TIM1 interrupt took place, inside
* HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment
* a global variable "uwTick" used as application time base.
* htim : TIM handle
* @retval None
*/
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
/* USER CODE BEGIN Callback 0 */
/* USER CODE END Callback 0 */
if (htim->Instance == TIM1) {
HAL_IncTick();
}
/* USER CODE BEGIN Callback 1 */
/* USER CODE END Callback 1 */
}
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* file: pointer to the source file name
* line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
Please inform me if possible.
I am attaching the main.c file kindly check it.
IDE - STM32cubeIDE 1.15.0
Board - STM32F401VC Discovery Kit
Thanks & Regards
Satyabrata Senapati(Firmware Engineer)