Does anyone have a recent TCP/IP project for a NUCLEO-H755ZI-Q generated by Cube MX 2.0?
Good evening,
I have been trying to get the ethernet port of my NUCLEO-H755ZI-Q to talk to my PC - and have been failing to do so now for a week.
I found this manual, but it is for Cube IDE 1.9 - and even after following the described steps I fail to talk via ethernet.
I did also find this github repo where I used STM32H7-LwIP-Examples/STM32H745_Nucleo_M7_ETH - and after adapting the IPs somewhat communication via UDP did work.
So I am rather sure my hardware does work.
But the code generated by CubeMX 2.0 does not.
Can anyone provide me with either
- a short manual how to configure CubeMX correctly,
- a ready-made example project using the current CubeMX 2.0,
- or any other input?
The current problem with my CubeMX 2.0 generated project is that during reception I get an
ETH_DMACSR_RBU /* Receive Buffer Unavailable */inside the
HAL_ETH_ErrorCallbackEn- or disabling ICache, DCache and MPU did not have any effect. I did move the RX_POOL to 0x30040000 as per the article and adapted the linker script. All to no avail.
Any help will be appreciated.
Thanks in advance
Johannes